10/29/2012 2:17 PM | |
Posts: 767 Rating:
|
Hello leszkoo, As confirmation of your inquiry, the 1FT6 synchronous motor (1FT6084-xSK7x-xPxx) can not support extended safety functions. The digit with P in above part number specifies the encoder type included internal to motor. The "P" specifies a resolver type of encoder. The extended safety functions require safe sensing of the position values on a drive(due to needs of redundancy). Resolver feedback type does nothave necessary redundancy for extended safety functions. For 1FT6 motors, this digit must be of type encoder that has incremental encoder or absolute encoder with photoelectric sampling can be used for safe sensing of the position values on a drive. For 1FT6 motors this digit must be an A, E, D, or F to be capable of supporting extended safety funtions. Please refer to attachment for further illustration. Best Regards, Deputy Attachmentextended safety.pdf (832 Downloads) |
Last edited by: O_Moderator at: 10/29/2012 2:22 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on