12/13/2022 8:03 AM | |
Joined: 1/21/2013 Last visit: 9/7/2025 Posts: 4090 Rating:
|
Hi, yes, C-PLUGs are supported. As you can see in chapter 4.2 of the operating instructions "SIMATIC NET: Industrial Ethernet security SCALANCE SC-600", C-PLUGs with 32 MB (6GK1900-0AB00) and with 256 MB (6GK1900-0AB10) are supported. The 32 MB variant, however, only for firmware version prior to than V2.2, because otherwise there is not enough memory space for the function "Firmware on PLUG". But there is no C-PLUG included, you have to order it separately. Kind regards |
Follow us on