9/20/2022 9:47 PM | |
Joined: 9/11/2022 Last visit: 8/4/2023 Posts: 4 Rating:
|
I have MOXA modbus gateway (modbus RTU to Modbus TCP) which connects power meter in series using RS-485 all the meter have same Serial port setting with different ID's. Modbus tcp has a unique ip address and TCP port:502. With every other software like KEPSware and MODSCAN all the devices communicate and gives data with same configuration except slave id. So there is no problem in commuincation. But in SICAM PAS when i create a modbus Master interface and add two devices only one communicate while other show connection error and when i stop the working one and start the other one the previous working one shows communication error. Also if the create a new interface and add the non working device, it start communicating. SO MY QUESTION IS DO i have to create new interface for each device connected on the gateway or is there any other solution b/c i have almost 90 devices on 6 gateways?? NOTE: i am using trial version of SICAM PAS for now to test my hardware. Also all the above stated devices show proper data on SICAM PAS if confiqured seperately so issue on address or any other things ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/21/2022 04:06:26New subject after splitting |
|
9/22/2022 6:41 AM | |
Joined: 10/9/2007 Last visit: 8/18/2025 Posts: 1281 Rating:
|
Hi nice picture post the wireshark log |
Energy Automation products: Sicam, Siprotec, Digsi |
|
9/24/2022 5:23 AM | |
Joined: 9/11/2022 Last visit: 8/4/2023 Posts: 4 Rating:
|
PC ip: 192.168.10.190 modbus Gateway.ip:192.168.10.191 modbus rtu devices address: 5 and 6 Procedure to capture packets: Start project->start Modbus Interface->Start Interface-> Start device 1 (connection helathy with data recieving) ->Start device 2(connection error) -> Stop device 2 and start again multiple times (connection error) -> Stop device 1 and 2 ->Start device 2 (connection helathy with data recieving)->Start device 1(connection error) -> Stop device 1 and start again multiple times (connection error). AttachmentPackets.zip (561 Downloads) |
Follow us on