4/30/2024 7:28 AM | |
Joined: 9/5/2019 Last visit: 9/12/2025 Posts: 4 Rating:
|
Dear Sirs, In order to connect to a DC load, I have to make sure that the output voltage is correct and stable. If Side 2 is open, Voltage control mode is selected, it is working with side2 open. If I connect a resistor to be a load to form a loop, there is no chance to start up successfully. It is same with current control mode. My question is: is it not possible for SINAMICS DCP to connect to a resistor load and start up directly? Attachmentdcp connection.pdf (619 Downloads) |
5/8/2024 1:08 PM | |
Joined: 4/24/2008 Last visit: 1/15/2025 Posts: 213 Rating:
|
I suggest to ask the customer support by opening an support request. |
|
|
Follow us on