2/29/2012 10:28 PM | |
Posts: 64 Rating:
|
I'm not sure about Siwarex but why not try running it under Windows virtual PC XP mode? |
3/1/2012 2:48 PM | |
Joined: 1/4/2007 Last visit: 8/26/2025 Posts: 1190 Rating:
|
Hello ememka, The software into the folder “SET_UP_FOR_SIMATIC_S7” is old and not valid for Step7 V5.5. You have to uninstall this old software from your Windows system and install the HSP-software for the Siwarex FTA module into the Hardware Configuration of Step7. You can find the HSP-software on the current configuration package CD of the Siwarex FTA module. For further information you can also contact the Siwarex Hotline. The email-address of the Siwarex Hotline is: hotline.siwarex@siemens.com. Best regards Siwarexi |
Last edited by: Siwarexi at: 05.09.2012 10:51 |
|
12/14/2012 4:09 PM | |
Joined: 1/4/2007 Last visit: 8/26/2025 Posts: 1190 Rating:
|
Hello nikolascha, Please contact the Siwarex Hotline and describe your problem. The guys will help you. The email-address of the Siwarex Hotline is: hotline.siwarex@siemens.com. Best regards Siwarexi |
3/17/2014 1:34 PM | |
Posts: 206 Rating:
|
Hello, just an additional information.It looks as if the problem comes from the integration of the Siwarex FTA into the HW-catalogue of S7.Therefore you have to install a new HSP to you system.The HSP you can find in the actual configuration package order no. 7MH4900-2AK02, there you find also the Siwatool for Win7.The HSP you can also download from here: http://support.automation.siemens.com/WW/view/en/79972902 !! Before you install the HSP you have to uninstall the old integration. Therefore you go in Windows to ControlCenter/Software and search for an entry like “SIMATIC Siwarex FTA…” and uninstall it. !!After this you can install the HSP like described in the FAQ. Regards ABenno |
Follow us on