4/2/2008 3:34 AM | |
Joined: 2/18/2008 Last visit: 4/4/2008 Posts: 11 Rating: (0) |
Hey guys, I have uploaded a circuit with 2 inputs and 2 outputs such that whatever is the sequence of the inputs, whenever the specific input button is pressed, the output will immediately switch to its corresponding operation. The problem that I am facing is to have multiple inputs. For example, if I want to have 3 inputs then I am not able to create such a circuit which satisfies the above condition. Can you guys tell me on how should I proceed after this circuit? Regards sahilg. Attachment2 inputs and 2 outputs.zip (828 Downloads) |
4/4/2008 4:00 AM | |
Posts: 191 Rating: (58) |
Hi!! Im not sure i understand what you arelooking for... please try this diagram and post your comments Hope this helps!! ROSA Attachment4 in 4 out.zip (745 Downloads) |
Follow us on