4/7/2023 5:48 AM | |
Joined: 10/19/2016 Last visit: 7/11/2025 Posts: 316 Rating:
|
Good morning sirs, i'm commissioning a milling spindle and I'd like to ask you an opinion about the attached graph and parameters after the auto-tuning. I get weird vybrations between 1700-2400 rpm but i'm not sure they're related to the motor. In any case I can see "excessive fluctuations" and a change in phase between 20 and 30 Hz in the position loop lower diagram. Is there any reference to tune the axis? AttachmentBinder1.pdf (325 Downloads) |
𓋹 Siemens 840Dsl + TIA v17 𓋹 |
|
Follow us on