4/17/2024 10:45 AM | |
Joined: 4/29/2017 Last visit: 5/1/2025 Posts: 47 Rating:
|
Hello , Dear friends ı need solution like Mr.Cetkin to store process values to scada I use s71500 cpu and Wincc Professional or Wincc 7.5 as Scada in my systems Problem is that ; I am logging process values from PLC to SCADA but some cases when PLC and SCADA connection aborted ( because of network problem or scada shutdown) process values cannot store to SCADA (SQL) in this case I want to store values inside of plc and if the connection state is healty then write back values to PLC to SCADA with releated timestamp and values(disconnected period of time and values) I reviewed energy suite dokumantation above , Could it be solution to my case ? Values that I store are not energy based but could it use different way ? As a result ı need solution to equlize PLC and SCADA values when connection disconnected Thank for advice... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/18/2024 07:50:46Text formatting optimized. Last edited by: Jen_Moderator at: 04/18/2024 07:52:44New subject after splitting |
|
4/25/2024 5:47 AM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16423 Rating:
|
Hello mittech as I wrote in the other topic, you could try to work with compressed taglogging archives to get aggregate functions or you have a look at this example: https://support.industry.siemens.com/cs/de/en/view/109739775 you can use compressed Taglogging data in the same way as common taglogging data Bye Murof |
Last edited by: Murof at: 04/25/2024 05:48:19If this Information really helps, you could use the Rate function |
|
Follow us on