1/21/2020 3:52 AM | |
Posts: 1 Rating:
|
Hi I have the same problem with a V90 PTI mode IPOS, fail F7492 or F7491 / I did test wiring CWL and CCWL to 1L or forcing to 1L, but the problem is the same when I try to move the motor. example position setpoit channel 0 value 10000 from reference point 0 Making with v-ssistant the test-motor / position trial run / the fail is the same I update the servodrive firmware, and the problem is the same It seems as the function IPOS in the servodrive not process the state of CWL or CCWL Please siemens i will apretiate a lot your support ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/21/2020 11:41:27New subject after splitting |
|
Follow us on