12/28/2018 4:02 PM | |
Posts: 9 Rating:
|
The HMI that I'm working with is version 6 while there is no version 6 in TIA. How can I add the version to the TIA? Thanks |
12/28/2018 4:43 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Have you seen this link: How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2? When you update the firmware in HMI, you can use TIA Portal WinCC Comfort to program. (That will be much easier Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
12/28/2018 4:50 PM | |
Posts: 9 Rating:
|
So you mean after the firmware update of the HMI, The version of it will be updated for example from 6 to 12? and then I can use TIA for it? |
12/28/2018 4:56 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
hello, yes this is the meaning. Regards Christoph |
This contribution was helpful to
1 thankful Users |
12/28/2018 5:00 PM | |
Posts: 9 Rating:
|
Thank you for all your answers really helpful. So can you help me how to update my HMI frameware? Thanks |
12/28/2018 5:03 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Have a look at the following link: Best regards, Wizard |
Follow us on