5/4/2016 8:39 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Paprima the PC Adapter USB is not a good way to load the Comfort Panel, its not released for this at all. I would use Ethernet or USB to download the Program. Perhaps you can do a test with this. It s also much faster than Profibus. If your Panel is connected over Profibus you can also use Project Transfer over Ethernet using Routing over the PLC. Here a few help for Transfer: https://support.industry.siemens.com/cs/ww/en/view/58522603 https://support.industry.siemens.com/cs/ww/en/view/58668002 If there are also Errors you should use OS update with Reset to Factory Settings over MAC Adress: https://support.industry.siemens.com/cs/ww/en/view/19701610 Good luck Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on