7/31/2025 7:10 AM | |
Joined: 7/24/2024 Last visit: 9/4/2025 Posts: 71 Rating:
|
Hi, PUT/GET is available on all access levels except "No access (complete protection)", which is the standard access level since the configuration via "Users and roles" became mandatory. To change the access level you have to assign the corresponding runtime rights to the user "Anonymous" and activate that user. You can find a description in this FAQ: How do you activate PUT/GET access on an S7-1500 CPU from FW V3.1 or S7-1200 CPU from FW V4.7? |
This contribution was helpful to
2 thankful Users |
Follow us on