4/22/2022 9:46 AM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello SrP3L4 The functionaliy of the GMsgFunction you can also use in WinCC Prof. in the properties of the alarms you can use the Event "Status changed" its basically the same as in WinCC V7 Here you have to use a C Script with the MSG_RTDATA_STRUCT Datatype as parameter. you could use the template of this FAQ also for the needed C Function in WinCC Prof: http://support.industry.siemens.com/cs/ww/en/view/15350783 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on