10/27/2018 6:57 AM | |
Posts: 1 Rating:
|
Hi, I have a Simatic logon V1.6 installed in a server and client having IPC 277E with Windows 10 and Wincc Flexible 2008 SP5. I am getting issues of conectivity to the server from client if i select TLS secured connection in Simatic logon congiguration and Encrypted transfer in Wincc Flexible sp5. But if i select a non-secured connection in configuration for simatic logon and deselect Encrypted transfer in wincc fexible sp5, then the connectivity is possible. i have few questions which i am not sure of: 1) why TLS secured connection is not getting established. (i created .pem certificates from openssl and configured. even selected encrypted transfer in Wincc flexible sp5) 2) What are the issues if we use non secured connection instead of tls secured connection.. any intermittent connectivity issues or anything??? i hope i put my doubts clearly. awaiting reply thanks Himan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/29/2018 9:35:38 AMNew subject after splitting |
|
Follow us on