10/30/2023 11:31 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi Alsandare, To see if there may be compatibility issues, it would be interesting if you could please attach the following information: - Capture the exact operating system version. To do this, you can write "winver" (without the quotes) in the Windows search engine and send us a screenshot showing which version and build appears. - I understand, to confirm, that you are installing WinCC V7.4, as you mention in the ost. - If there is any error or message that you get when the installation fails, it would also be important. Best regards!
|
If this Information really helps, you could use the Rate function |
|
10/31/2023 9:16 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Alsandare you can check for your own if there are any compatibility issues: https://support.industry.siemens.com/cs/de/en/view/64847781 2016 Standard (64-Bit) and 2016 Datacenter (64-Bit) is only released with WinCC V7.4 SP1 not without SP Bye Murof |
If this Information really helps, you could use the Rate function |
|
11/7/2023 1:52 PM | |
Joined: 5/15/2021 Last visit: 7/13/2025 Posts: 3 Rating:
|
Well, how to install if it does not allow installation, where can I get an installer with SP1 enabled?https://ibb.co/wrsxgH8 |
Last edited by: Jen_Moderator at: 11/10/2023 12:38:00Text formatting optimized. |
|
11/10/2023 12:39 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Hello Alsandare, please attach your files as an attachment and don't use ibb as a filesharing hoster. I can't open and check it, because the website is blocked. If you want to attach more than one file, you can create a zip file. Best regards, |
Follow us on