2/4/2017 1:02 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: In this sample, a controller's user program Program_alarm block call will generate a message on a HMI. Alarm messages are an important tool for operation diagnose of process and system events. The possibility to generate messages directly from the controller's blocks reduces the HMI configuration time. The same main steps are also applicable to WinCC Advanced / WinCC Professional. Requirements: WinCC Comfort V14. Configuration main steps: On Controller side: Create a block (Block_1)
On HMI side:
References: /1/ WinCC Advanced V13 SP1 – Simple Sample: Invert Bit Help system for Program_alarm block (F1) Project: Archived program, compressed (zip) AttachmentProject1.zip (313 Downloads) |
Last edited by: Denilson Pegaia at: 2/4/2017 1:29:29 PMDenilson Pegaia |
|
Follow us on