4/16/2009 11:58 AM | |
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
Hello together, first: WinCC flexible 2007 should not be used with WinXP SP3 ( see here!! ) and then there is only one way to open this project in WinCC flexible 2007: you have to give the project back and then it must be saved in Version... ( see this FAQ ) you don´t have more possibilities to open this projekt with WinCC flexible 2007... regards manfred |
4/16/2009 1:16 PM | |
Posts: 2 Rating:
|
I do have those 2 files in the project directory. I will try to see if the project can be downgraded. Thanks for the help! |
Follow us on