7/18/2017 9:45 AM | |
Joined: 8/3/2009 Last visit: 9/9/2025 Posts: 16358 Rating:
|
Hello Gregus Zsolt to 1.) With a WinCC Professional RT License there are up to 8 connections licensed and you can use the softnet License with a normal ethernet card (Softnet). You need no forther license or Hardware to2.) with WinCC Advanced RT you can only use 8 connectoins and you do not need another License only for communication. you just have to check your Powertags and if you use Recipe or Logs or Options. You can use a normal PC Ethernet Card. But be sure the S71200 have only few communication ressources. check this FAQ: https://support.industry.siemens.com/cs/ww/en/view/109479986 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
Follow us on