9/18/2009 8:05 PM | |
Posts: 2661 Rating:
|
The server should be in runtime. Standard pictures that got copied from bin when you inserted the client application will get transferred to the client station during downlaod. All other process pictures (user created) will be read from the server. Do you have OS Project Editor Option? If yes, run this in client project (on server) before downloading project to client. Also, you can try to create a client project manually and load server data and activate runtime. This will be a good test. Regards Update Also see the following thread: Wincc Server Client Connection Problem |
Last edited by: Phantom75 at: 9/18/2009 10:42 PM |
|
Follow us on