8/5/2024 8:25 AM | |
Joined: 11/21/2020 Last visit: 9/11/2024 Posts: 145 Rating:
|
Hi, Can you advice the easiest way to control Stepper Online CLT57 stepper drive ? Stepper Drive's CLT57 V4.0 manual is attached. Thanks AttachmentCL57T V4.1 Manual.pdf (36 Downloads) |
8/5/2024 10:09 AM | |
Joined: 3/30/2020 Last visit: 9/11/2024 Posts: 4743 Rating:
|
Some things are marked in yellow in the manual you shared. Figure 6 among those. The confusion is that it is unclear if all the electrical connections are already completed. Why is the drive manual shared with the forum? The easiest way for the S7-1200 to control a stepper motor is to use motion control via pulse and direction. Have you done that before? Have you studied the motion control manual for the S7-1200? (A5E03790551-AG) The MC_Power + MC_MoveJog instructions are all you need to make the stepper motor run with a user program. Provided the motion control has been configured with the help of the technology object wizard. Please spell out what your needs are. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
8/5/2024 1:51 PM | |
Joined: 3/30/2020 Last visit: 9/11/2024 Posts: 4743 Rating:
|
This question is posted in the conference relating to the S7-1200 hardware. That opens the question if you have a hardware question. But it could be related to Simatic Technology (motion control instructions).
It is not possible to know what type of help you need if you do not interact with the questions I have asked. From your response it is too easy to assume that you will study the link I posted and come back for clarity. Some self study materials.. Specifically to the S7-1200 Generally about control; including drives control |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on