6/4/2024 12:26 PM | |
Joined: 6/1/2022 Last visit: 6/17/2024 Posts: 26 Rating: (0) |
The modules are all functioning normally, with status LEDs all green. The addresses used are automatically configured when we add the rack modules, QW6, QW8, QW10... QW20. I'm using the norm-x and scale-x blocks to convert 0-100% into 0-27458 in an OB30, different from the main one (OB1), where I put the values between 0 and 100% manually through tiaportal in online mode and check that the output receives the equivalent value (if I add 30% the output receives 8520) and I am using 0-10V outputs, I have already configured the modules to send voltage.
AttachmentScreenshots.zip (314 Downloads) |
Last edited by: Jen_Moderator at: 06/05/2024 07:19:14All files added as .zip file. |
|
Follow us on