3/15/2006 1:51 PM | |
Posts: 5822 Rating: (412) |
Hello, I would say it should work as it is explained here: http://support.automation.siemens.com/WW/view/en/12714722 in Chapter 2. Best regards. J_Bell |
3/17/2006 2:14 AM | |
Posts: 29 Rating: (0) |
[quote user="Pegaia"] Hi, I don’t know exactly what happens but I have some suggestions / question: 1 – Is there a MMC card on the IM-CPU? 2 – Is the MMC leer or has a wrong configuration inside? 3 – Have you tested MPI with the option only master on the bus? 4 – Have you tested to use the option MPI/PB (auto)? 5 – Have you tested to use the option Diagnose of PG/PC interface (only for PROFIBUS)? 6 – What cable are you using? This cable works with other CPU? 1. Yes there is. 2. Not sure. 3. Yes 4. Yes 5. No profibus card. 6. MPI cable, Yes it works for my s7-300 plc. Here are some pictures. http://i6.photobucket.com/albums/y230/Fatty1234/pic1.jpg http://i6.photobucket.com/albums/y230/Fatty1234/pic2.jpg http://i6.photobucket.com/albums/y230/Fatty1234/pic3.jpg http://i6.photobucket.com/albums/y230/Fatty1234/pic4.jpg |
3/20/2006 7:49 AM | |
Posts: 29 Rating: (0) |
Thanks Pegaia and J_Bell for helping me out [:)]. Now i am able to download and view the module information. But it seems that there is an error as shown in this link http://i6.photobucket.com/albums/y230/Fatty1234/pic6.jpgwhich i am unable to clear/reset it.[:(] I have alreadycontacted my tech support. While waiting for their reply, was hopping anyone could help out. Thanks. |
Follow us on