6/11/2014 8:28 PM | |
Joined: 8/16/2010 Last visit: 11/5/2024 Posts: 638 Rating: (12) |
Hi all... How can I connect Burkett batch controller electronics SE35 (manual attached) with pulse output to PLC? I think that I need to connect pulse output from controller to HSC? Every suggestion is welcome. Thank's AttachmentDS8035-Batch-EU-EN.pdf (633 Downloads) |
6/11/2014 8:43 PM | |
Joined: 8/16/2010 Last visit: 11/5/2024 Posts: 638 Rating: (12) |
Datasheet
AttachmentMA8025-8035Standard-EU-EN.pdf (678 Downloads) |
6/12/2014 7:19 AM | |
Joined: 8/16/2010 Last visit: 11/5/2024 Posts: 638 Rating: (12) |
Thank's. But I'm little bit confused. On Fig 21. on PLC side I have + and - 5-36VDC? I need to connect P+ output of the device to HSC input of PLC, and P- from 0V of my power supply. (see attached doc.) Specification: frequency is from 0.6 to 2200Hz, HSC is 100Hz. Is that essential for accuracy of flow? How to handle that on TIA side? Attachmentpulse.pdf (677 Downloads) |
6/12/2014 12:29 PM | |
Joined: 7/7/2010 Last visit: 11/19/2024 Posts: 15406 Rating: (2446)
|
HSC is up to 100kHz which is plenty of counting capability for your device. |
science guy |
|
6/12/2014 12:33 PM | |
Joined: 8/16/2010 Last visit: 11/5/2024 Posts: 638 Rating: (12) |
Oh yes...my fault. Thank's huggy. Is my wiring diagram from previous post ok? |
6/12/2014 12:46 PM | |
Joined: 7/7/2010 Last visit: 11/19/2024 Posts: 15406 Rating: (2446)
|
At a glance if looks like exactly how I would expect it to work. |
science guy |
|
6/12/2014 12:57 PM | |
Joined: 8/16/2010 Last visit: 11/5/2024 Posts: 638 Rating: (12) |
OK...Thanks a lot. |
Follow us on