1/30/2023 8:45 AM | |
Joined: 10/11/2006 Last visit: 8/7/2024 Posts: 5887 Rating: (802)
|
Hello, you can directly change the value in your program code. "<TO>.DynamicLimits.MaxVelocity" MaxVelocity LREAL 0.0 … 1.0E12 RES Maximum permissible velocity of the axis RES Restart: Changes to the start value in the load memory are made using the extended instruction "WRIT_DBL" (write to DB in load memory). Changes will not take effect until after restart of the technology object. 9.2.16 "DynamicLimits" tag (positioning axis) (S7-1500, S7-1500T) MaxVelocity LREAL 0.0 … 1.0E12 RES Maximum permissible velocity of the axis https://support.industry.siemens.com/cs/ww/en/view/109812057 |
With best regards, |
|
1/30/2023 10:36 AM | |
Joined: 3/3/2014 Last visit: 7/22/2024 Posts: 234 Rating: (9) |
Hi @Technology Team , Thanks for you answer, I Will try today and let you know. Also , couple of things: 1) What's going on, if I change the Start value directly, in the DB Istance of technology object in "<TO>.DynamicLimits.MaxVelocity" and then, reload the PLC ? 2) When I restart the Technlogy Object using, the MC_RESET block, and then RESTART , Do I have to redo the zero as well, or does the position remain stored? Thanks
|
2/9/2023 3:16 PM | |
Joined: 10/11/2006 Last visit: 8/7/2024 Posts: 5887 Rating: (802)
|
Hello, 1) What's going on, if I change the Start value directly, in the DB Istance of technology object in "<TO>.DynamicLimits.MaxVelocity" and then, reload the PLC ? //After download it is active.
2) When I restart the Technlogy Object using,the MC_RESET block, and then RESTART , Do I have to redo the zero as well, or does the position remain stored?
5.7.10 Resetting the "Homed" status (S7-1500, S7-1500T) Incremental encoder In the following cases, the "Homed" status is reset, and the technology object must be rehomed. • Error in sensor system/encoder failure • Starting an "MC_Home" job with "Mode" = 3, 5, 8, 10 (As soon the homing mark has been approached, the status "Homed" is set to "TRUE".) • Replacement of the CPU • Replacement of the SIMATIC Memory Card • POWER OFF • Memory reset • Modification of the encoder configuration • Restart of the technology object • Restoration of the CPU factory settings • Transfer of a different project into the controller When you use a new incremental encoder you need to home the incremental encoder once again. Absolute encoder In the following cases, the "Homed" status is reset, and the technology object must be rehomed. • Replacement of the CPU
• Changing the encoder type to incremental encoder
• Restoration of the CPU factory settings
• Transfer of a different project into the controller
When you use a new absolute value encoder you need to home the absolute encoder once
again.
Resetting the memory of the CPU or upgrading a project does not require another absolute
encoder adjustment. https://support.industry.siemens.com/cs/ww/en/view/109812057 "WRIT_DBL" is only used for changing via programm. |
With best regards, |
|
Follow us on