2/15/2011 8:17 AM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi again, So I went further and got back up from MasterDriveMcPlus, but In Drive Monitor diagnostic I got some errors/faults time to time Master Drive MC+model is here: 6SE7018-0EP50-Z and Z= (C23+G91+F01) Drive monitor ask database when I clickfault code, is there some database somewhere to connect/import?? Faults which I have here in diagnostig window: 82 TB/CB tlgr 1 027 UCE L3 042 Compute tim Examble: when this 042 fault came MasterDrive MC´s panel shows A001, F042 and A008, need to reset before working again. Before Master Drive there is MASTERDRIVES RFI (radio interference suppression filter) 6SE7021-2EP87-0FB0 Splitted from I need to upload Masterdrive parameters and see diagnostic and faults and alarms. |
Last edited by: O_Moderator at: 2/16/2011 8:58 AMnew subject after splitting "Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
Follow us on