6/26/2024 6:59 AM | |
Joined: 9/28/2022 Last visit: 10/4/2024 Posts: 32 Rating: (0) |
Hello, I am using Proxmox hypervisor and I'm trying to get CP1623 to passthrough to a virtual machine. This far I've got it to register in device manager in the VM and in adapter settings i also see it, but it fails to startup in Station Configurator with error 0x0381, the exact message is as follows:
Cant seem to find much information on it, this is for virtualisation of PCS 7 system, 2 redundant servers 1 ES, this is only for virtualisation test so far so i can do whatever. I have 3 CP1623 in the host machine, 1 for each. i attached my PCI connected devices as file "pvesh get.txt" At the start I was not really sure which device to passthrough as theres 2 devices linked in slot x (19-22) but after fiddling a bit i found that the ones named "MPC8347 PBGA" are the ones i wanted to passthrough, but I'm not 100% sure this is correct setup, does anyone have any experience with this? For example further information on error 0x0381 I cant find much, or PCI passthrough of CP1623 Further information: Attachmentpvesh get.txt (208 Downloads) |
8/20/2024 8:35 PM | |
Joined: 8/7/2024 Last visit: 9/13/2024 Posts: 1 Rating: (0) |
Hello. can you confirm that CP1623 works correctly in a virtual machine using passthrough in proxmox? |
Follow us on