2/15/2022 5:03 PM | |
Joined: 3/27/2008 Last visit: 9/10/2024 Posts: 1133 Rating:
|
PC connection set, ref. 6SE6400-0PA00-0AA0 This is a connection kit for connecting a PC to the drive. The interface replaces the AOP onto the front of the drive. The serial cable, this connects to a PC running STARTER, this is a free download from the Siemens website. Serial ports on PC's are now rare, so a serial to USB converter may be required. 'Language Blocks', the AOP had a limited memory, to increase the available memory for uploading data sets from drives languages could be deleted! Once a language was deleted it could not be restored, this lead to many AOP's being without Languages and therefore unserviceable. AOP with corrupt set of parameters, this AOP may still work but the parameter set may not be available. Is the AOP still reading inverter parameters from a live MM440? I hope I have answered your query, but if not come back. Tractor AttachmentAOP.pdf (619 Downloads) |
Last edited by: Tractor at: 02/15/2022 17:10:47Tractor |
|
Follow us on