11/16/2022 7:13 AM | |
Joined: 1/21/2013 Last visit: 11/18/2024 Posts: 3283 Rating: (510) |
Hi PedroDias009, this question was also discussed in Differences between Professional vs Unified. To choose the right system, many factors are important. Among other things, it is a question of which control system is used for communication, what the alarm system must be able to do, whether recipes are required, what must be logged, and much more. I myself do not like to project an HMI or SCADA, I find the effort is too great and would like it to be easier. However, I myself see great potential in WinCC Unified and would rather rely on it for the future. However, since the range of functions is limited - even if it will soon be expanded by V18 - it would be advisable to have the requirements checked by the technical consulting. Nothing is more damaging than a failure shortly before the goal because a function is missing. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on