5/19/2024 6:46 PM | |
Joined: 5/22/2019 Last visit: 6/14/2024 Posts: 10 Rating: (1) |
I have a S120 democase like this one. I am trying to config a simple S7-1500 TO project with it, e.g. one positioning axis and one gearing axis. I was able to reach this far that everything is green in TIAPortal. I can move the axis in control panel. Looking at the diagnostics, and alarm messages, there are some hints on following error config. But it does not solve the problem even if I can that following error min value to any possible values.
|
Follow us on