10/8/2021 5:48 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS Forum Community, Our SIMATIC S7-1200/1500 controllers support the Modbus TCP protocol e.g. via the integrated PROFINET interfaces. To establish an access of measured data to SENTRON PAC devices there are already some interesting articles (FAQs, application examples) describing the access of a SIMATIC S7-1200/1500 to a SENTRON PAC device and the data preparation of the measured data e.g. with the option Energy Suite. See: 1. Data communication between S7-1200 and SENTRON PAC3200 via MODBUS TCP (Set 22). See: https://support.industry.siemens.com/cs/ww/en/view/40614428 2. SIMATIC S7-1500 Block for Integrating of Modbus TCP Devices into Energy Suite See: https://support.industry.siemens.com/cs/ww/en/view/109749074 However, if only one or a few values of the SENTRON PAC devices are relevant for the PLC, a solution can be found quickly with the SENTRON Communication Library for SIMATIC TIA Portal. The SENTRON Communication Library for SIMATIC TIA Portal can be found at the link: https://support.industry.siemens.com/cs/ww/en/view/109752144 The library is available for TIA Portal versions V15 and V16 and it contains HMI templates in addition to the product-specific communication blocks of the PLC. In addition to an illustrative demo project for the S7-1200/1500, the available library elements can also be individually integrated into existing projects in a product-specific manner. Best regards, SIMATIC International Technical Support Hub |
Last edited by: Jen_Moderator at: 10/11/2021 10:26:19Edited text for better reading. |
|
Follow us on