Industry Online Support
Technical Forum
5/28/2014 12:32 PM |
|
Posts: 202 Rating: (16) |
Hello Everyone What isInsulation Monitor?I came across this term during a retofitting job.please help me out
|
5/28/2014 12:56 PM |
|
Joined: 5/12/2014 Last visit: 9/9/2020 Posts: 149 Rating: (16) |
Dear @nkur, Aninsulation monitoring devicemonitors theungrounded systembetween anactive phase conductorandearth. It is intended to give an alert (light and sound) or disconnect the power supply when theresistancebetween the two conductors drops below a set value, usually 50 kΩ(sample of IEC standard for medical applications). The main advantageis that the ungrounded or floating system allows a continuous operation of important consumers such as medical, chemical, military and etc. Even if there is a failure (i.e., phase touches ground) there is still no danger to the personnel and to the application.
|
5/29/2014 12:59 PM |
|
Posts: 235 Rating: (52) |
Dear, Please folloe this Link |
5/29/2014 6:06 PM |
|
Posts: 202 Rating: (16) |
HI there Is it necessay to have OHM value in kilos??also what do you mean byEven if there is a failure (i.e., phase touches ground) there is still no danger to the personnel and to the application???
|
Follow us on