9/3/2025 6:41 AM | |
Joined: 3/11/2009 Last visit: 9/13/2025 Posts: 6 Rating:
|
Hello bg2492, I'm trying to migrate a WinCC project from WinCC v6.0 to WinCC v8.1. The migrated project to WinCC v7.2 works without errors. The cross-referecing is the same and correct. When I open a migrated project from WinCC v7.2 in WinCC v7.5 or WinCC v8.1, the cross-referencing throws an SQL exception.
System.Exception: System.Data.SqlClient.SQLException (0x80131904): Invalid column name ‘HidingVarID’….
I tried using your query (but 0 rows affected). I tried deleting content from tables as you suggested (the same i found on support siemens) Still without success. Can you give me some advice? Thanks
------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 09/03/2025 12:57:23New subject after splitting |
|
9/4/2025 6:54 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello jozjo first I would recommend using the latest Updates available for your WInCC Version https://support.industry.siemens.com/cs/de/en/view/109818723 Then open the Project from the previous version and then Tools->"Convert Project data" go to the project folder and check if there is a folder CROSSREF if yes is there something inside? Try to delete the content of the folder and open the crosrefference in WInCC again Does it also occur with a new test project? -> If the error lasts then you can also try to open as Service Request, perhaps the project is damaged somehow Bye Murof |
If this Information really helps, you could use the Rate function |
|
9/10/2025 11:21 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello jozjo does is only occur with this special project or also if you create a new test project and try the crossref? LINKIf also the troubleshooting with the databases do not work (LINK) then perhaps the project is damaged. In this case you should open a Service request at Siemens Support Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on