5/15/2025 1:05 PM | |
Joined: 9/16/2024 Last visit: 5/26/2025 Posts: 1 Rating:
|
Hello, my name is Mauro and I have the following issue: When I power off and on the PLC, it loses the current position. I need to perform position control, for which I’m using Telegram 3 and have configured the drive in V-ASSISTANT with "Speed Control Mode", since I understand that the positioning is handled by the PLC and not by the drive. I’m performing the positioning using Motion Control blocks (MC_POWER, MC_RESET, etc.). Here is a description of the hardware and software involved:
I’ve attached some screenshots of the technology object configuration. Attachmentimg.pdf (217 Downloads) |
Last edited by: AutoGen_1642978 at: 05/15/2025 13:10:23Last edited by: AutoGen_1642978 at: 05/15/2025 13:11:38 |
|
Follow us on