1/10/2024 11:46 AM | |
Joined: 7/19/2022 Last visit: 10/18/2024 Posts: 403 Rating: (65) |
Hello Erik Skou, If you are using the default viewer to log in you will not be able to do much since it is a system window that cannot be modified. If you are doing it with your own fields, you will have an I/O field associated with a variable that stores the name, therefore, it is normal for that field to show the last value that the tags has. |
If this Information really helps, you could use the Rate function |
|
1/11/2024 8:41 AM | |
Joined: 11/1/2019 Last visit: 10/9/2024 Posts: 5 Rating: (0) |
Thank you for the answer. |
Follow us on