9/11/2025 11:26 AM | |
Joined: 3/4/2024 Last visit: 9/11/2025 Posts: 2 Rating:
|
hi i am also facing same issue with TIA V20.MY CPU IS COMPACTIBLE ONLY TIA V20 .BUT NOT ABLE TO DOWNLOAD THE APPLICATION INTO HMI VIA TIA 20.AND MY HMI IS SIMATIC COMFORT PANEL TP1500.6AV2124-0QCO2-OAX1.PLS FIND THE ATTACHED SCREENSHOT. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_5144333 at: 09/11/2025 11:26:50Last edited by: Moderator_Lan at: 09/11/2025 12:48:11New subject after splitting |
|
9/16/2025 8:25 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16439 Rating:
|
Hello like the messages indicates you need the correct Panel Image. you can use the PIU Installer from this LInk or also the offline Installation if there are problems with the PIU: https://support.industry.siemens.com/cs/de/en/view/109825750 Check in your HMI Device which Device Version you have set also. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on