7/30/2008 2:23 PM | |
Posts: 24 Rating:
|
Strickly speaking you do not have to update the HW configuration to update your FMs. We have done it both ways: (Just replacing the FM - and putting the old MMCcard in the new FM), and (Doing the HW change over, downloading, swapping MMC card and installing FM, recompiling and reloading software based on possible library changes.) The second option is the most correct. The only other software updates that we had to do to see the new FM in the HW config were: 1. Update D7-SYS to SP2 Download Here: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=24367507&caller=view 2. Then add Hot Fix #1 to D7-SYS SP2 Download Here: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=24623387&caller=view (Should do this on every programmer you have) NOTE:!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!! By updating D7-SYS you will be forced to update the libaries that you are using in CFC. You will know right away when you try and compile the FM in CFC, it will give lots of errors. Simple Procedure for this: 1. Open Project in CFC 2.In the Compile Settings, select the option “System data from Installation”. Select Okay. (This will force the CFC compiler to look at the local libraries while updating.) (Do NOT Hit Clear Libraries.) 3. Inside CFC, select menu: Options->”Block Types” All of the libraries that were just updated by the service packs need to be re-imported. Select each of these new libraries in the left hand window that corresponds to and older version of a library in the right hand window and select the button “New Version”. (For Example: If FBSFM1 is version 102500V616 in the “Imported libraries” tab and it is version 102500V 617 in the “Installed Libraries”, then click the FBSFM1 in the “Installed Libraries” and click the button: “New Version”.) 4. Compile and Download the FM again. 5. In the Compile Settings, select the option “System data from Archive”. This will store the local libraries in themaster project so they can be archivedwith your code. Makes life easier if you loose your programming PC. |
This contribution was helpful to
2 thankful Users |
1/24/2013 8:03 AM | |
Posts: 1 Rating:
|
Where can I find this "CFC manule"? thank you |
1/24/2013 8:31 AM | |
Joined: 8/25/2006 Last visit: 9/12/2025 Posts: 2218 Rating:
|
Hello. Do you mean CFC-menu or CFC manual?
|
Follow us on