7/10/2017 7:27 PM | |
Posts: 1 Rating:
|
Hello, I've written a program of analog output, using functions NORM_X and SCALE_X, And after I created an HMI screen for it (like linking tags to the i/o textbox etc.), I tried to run simulation to that HMI, and I got that error: " ,HMI_Connection_1: Local interface does not exist; Partner subnet is not connected.; Partner subnet is not connected.,,,8:25:24 PM" Does anybody knows how to fix that error? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/11/2017 1:20:56 PMNew subject after splitting |
|
7/12/2017 8:26 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
Hi, this error is reported during compilation of the HMI right? Go to the properties of the HMI Connection an check this. You also must check the IP Settings for the HMI and the PLC, You should also post some Screens of the Errormessage and of the configuraton you do in the project. Regards Christoph |
This contribution was helpful to
1 thankful Users |
8/14/2017 10:37 PM | |
Joined: 6/27/2016 Last visit: 4/3/2025 Posts: 11 Rating:
|
This has happened to me while using TIA Portal, adjust PG/PC interface to the protocol you are using in your simulation (Ethernet IP/ Profibus/MPI). Hope this solves it.
|
8/14/2017 10:38 PM | |
Joined: 6/27/2016 Last visit: 4/3/2025 Posts: 11 Rating:
|
also you might want to re-create the connection to the panel, maybe you set the wrong interface? |
Follow us on