11/4/2024 9:19 AM | |
Joined: 10/1/2015 Last visit: 9/1/2025 Posts: 22 Rating:
|
Dear all, i have wincc v8 upd5, and i have 10 connections TCP/IP to s300 and s400 plcs. and 8 OMS+ connections to S1200. Some of s1200 are old (madein TIA11, TIA12) some of them are in TIA17 with needed certificates for communication. Connecitions to OMS+ are droping and comming back. Any idea where is problem? [Attached] is part of diagnose: Attachment04.11 Diagnose.txt (146 Downloads) |
Last edited by: Moderator_Lan at: 11/04/2024 09:34:18Code attached |
|
11/5/2024 5:42 PM | |
Joined: 7/19/2022 Last visit: 9/1/2025 Posts: 436 Rating:
|
Hello djpiky, Do you have SIMATIC NET installed and if so, which license do you use? For more than 8 S7 connections, the SOFNET-IE S7 license is required.
|
If this Information really helps, you could use the Rate function |
|
11/13/2024 10:46 AM | |
Joined: 8/3/2009 Last visit: 9/1/2025 Posts: 16284 Rating:
|
Hello djpiky Check the communication ressources of your S7-1200 PLCs. the older ones do have problems connecting multible HMI Systems.Do you have another HMIs like Panels connected to this PLCs also? If yes disconnect them and look if this connection is stable in WInCC... https://support.industry.siemens.com/cs/ww/en/view/109479986 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on