11/27/2024 10:00 AM | |
Joined: 2/5/2023 Last visit: 8/30/2025 Posts: 23 Rating:
|
hi I want to use ssl certificate in client (cell phone or laptop) and client access to Wincc Webux pages only by certificate. So anybody that has not certificate can not access to Webux pages. I can see Webux pages in client with certificate and without it. But I do not know how to restrict user according to certificate owner. my PCs specification: wincc v8.0 in server windows 10 in both server and client I did this procedure from this link ( https://support.industry.siemens.com/cs/mdm/109773078?c=127750550283&lc=en-WW ) ; Procedure
4. To configure the settings, click "Add". The "Add site bindings" dialog opens 5. Select the website type, IP address and the port. To display the fields for configuration of the SSL certificate, select the type "https". 6. Select the SSL certificate from the list or with "Select". 7. Confirm with "OK" to close the dialog. You can delete the other entries in the "Site bindings" dialog. 8. Exit the configuration with "Close" 9. In the data area "Default Web Site Home", select the "SSL settings" under "IIS" 10. Activate the "Require SSL" option and select the setting for client certificates. |
Follow us on