9/14/2007 5:22 PM | |
Posts: 70 Rating: (3) |
The error could be caused by your hw configuration beeing inconsistent. This link explains a little bit about which step7 versions is compatible with the new v5 CPUs http://support.automation.siemens.com/WW/view/en/24222369 In any case I suggest that you download the newest hw support directly from the hw manager (options - install hw updates) The newest Step7 SP for v5.3 (SP3) can be found here : http://support.automation.siemens.com/WW/view/en/21953245 A complete list of SP's is here : http://support.automation.siemens.com/WW/view/en/10805386/133100 god luck Søren |
9/17/2007 5:25 PM | |
Posts: 20 Rating: (0) |
Thanks I downloded SP3 and now it works. |
Follow us on