6/3/2024 1:02 PM | |
Joined: 6/4/2010 Last visit: 9/27/2024 Posts: 387 Rating: (128) |
Dear Alex, There are several other parameters which have to be specified (application, flow, 2-point 24V / 230V or modulating with reset function etc.) in order to be able to select the best suitable valve actuator. I would recommend to either use the HIT tool under the link below:https://hit.sbt.siemens.com/RWD/app.aspx?RC=HQEU&lang=en&MODULE=Product&ACTION=ShowGroup&KEY=HIT_Prod_Grp_52799&VALUE=HoV Or contact the Siemens sales office in your country to find the right products for your needs. Best regards, Albis |
6/6/2024 3:15 PM | |
Joined: 6/4/2010 Last visit: 9/27/2024 Posts: 387 Rating: (128) |
Dear Alex, You may need the DVGW certificate for drinking water. You can find the range overview under the following link: https://sid.siemens.com/v/u/A6V10200220 Suitable valves are the MXG461B magnetic valve or the VXG41..01 for drinking water applications. See also in the HIT selection tool under: https://hit.sbt.siemens.com/RWD/app.aspx?RC=AT&lang=de&MODULE=Product&ACTION=Search&VALUE=DVGW Best regards, Albis |
Follow us on