4/29/2024 6:22 AM | |
Joined: 4/8/2024 Last visit: 10/17/2024 Posts: 5 Rating: (0) |
Hi bg2492, May I know if I can uncompress the binary packages via SQL script? The reason being is I am working on report designer, with intention to utilize ODBC table to display my compressed archive value from SQL database. ODBC table allow me to write the SQL query, which give me flexibility in designing my report layout. Now the only issue is I can't display my compressed value because it is shown in binary values. I have gone through the siemens example "Export of archive data using the SIMATIC WinCC/Connectivity Pack (OLE DB Provider)", but it required extra step to uncompress the data into CSV form, which is not suitable for me to directly read the data via ODBC connection. Any suggestions are appreciated. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/29/2024 12:00:34New subject after splitting |
|
Follow us on