6/27/2024 3:02 PM | |
Joined: 3/14/2008 Last visit: 7/2/2024 Posts: 2075 Rating:
|
Hi, You can rename the FC to another number in the Blocks folder of the AS project. Next, you have to change the FC number in the symbollist as well. You can do this with a compile+download change, but beware of the following. When another block like an FB is calling the FC, you will get an error while compiling. You have to make sure that this isn't the case, otherwise you have to compile the SCL/STL source as well and update to the project, which may cause a stop if TCiR cannot be used.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on