10/19/2023 9:37 AM | |
Joined: 11/26/2022 Last visit: 10/19/2023 Posts: 1 Rating: (0) |
Hello dear Mike. I have configured a Siprotec5 relay in Digsi5, exported the .scd file and imported it in SICAM PAS also I use IED Scout to simulate my Siprotec5 relay. I also made an HMI for it in SCC. the Communication Protocol is IEC 61850. I have assigned signals to SoftPLC in Mapping and I use PAS_ANDI, PAS_CRCOM and PAS_COMMCP to make the value of "c_CB_Control_Cmd_with_feedback" signal change so I can Command the CB to On or Off. The problem is: 1) I can only get 0 a 1 for the value of my Command while for Off it must be 1 and for On it must be 2. 2) the "CB_Control_Cmd_with_feedback" signal value which is Information of CB does not change with "c_CB_Control_Cmd_with_feedback". I'd appreciate if you can guide me through this. best regards. Saeid Akbari. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/20/2023 03:50:31New subject after splitting |
|
Follow us on