4/29/2010 7:20 AM | |
Joined: 3/24/2009 Last visit: 7/9/2024 Posts: 535 Rating:
|
Dear Phumula, which failsafe-system do you use (Distributed Safety of F-Systems)? I think it's Distributed Safety, right? If so, please start the 'Check for Accesses from the Standard User Program' - function (you find it in the 'Edit safety program' dialog at the arrow of the compile-button). I guess, that you write somewhere in the standard-program on values, which are used in the safety-program or call F-Blocks from the standard-program. Best regards, yy1 |
4/29/2010 9:25 AM | |
Joined: 10/7/2005 Last visit: 8/18/2024 Posts: 3016 Rating:
|
Hello Phumula perhaps these two links will be helpful too (applicable assuming you useDistributed Safety): S7 Distributed Safety V5.4 + SP2 has been recalled What should I do if the F-CPU goes into STOP mode and the message "Data falsification in the safety program ..." appears in the diagnostics buffer? |
Cheers |
|
Follow us on