11/22/2023 8:35 AM | |
Joined: 3/6/2014 Last visit: 8/20/2024 Posts: 78 Rating: (1) |
Hi, I want when the emergency button is pressed, the system should automatically deactivate the power supply to the output module and all outputs don't Voltage till don't reset emergency relay. I have drawn an electrical schematic diagram that I would like to discuss. I taken emergensy relay, output module 6ES7132-6BF00-0CA0 and BaseUnit BU15-P16+A0+2D. It is possible connect how I have drawn electrical diagram. Does is another solution? I'm not sure, but if I take power from the module, will the PLC generate an error since it doesn't detect the module? Attachment021-Model.pdf (305 Downloads) |
Follow us on