5/22/2016 6:34 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (874) |
Hello, Basically the drive & CU you mentioned are not G150 & CU 230. Drive is S120 & CU unit is 320. Plesae refer link 1 & link 2. Based on MLFB number you provide. Please just provide the MLFB numbers if you are not sure about the type of drive. Providing wrong information misleads the forum members who want to help you. Please let us know if this is single Motor module or multiple motor modules are connected in parallel? From your description, assuming parallel operation of motor module, let us know if the problem is displayed on this motor module? Please provide the MLFB number of infeed module. If the drive is operated on profibus, why TB30 option is used. Please check the control logic. |
5/23/2016 11:53 AM | |
Posts: 101 Rating: (1) |
P278 = 0 whats the definition of this parameter and if what can happen if we change it to another value. |
Follow us on