8/5/2024 2:44 PM | |
Joined: 6/6/2024 Last visit: 9/12/2024 Posts: 1 Rating: (0) |
I have made a HMI in WinCC and it works fine like yours. But when I see this in WinCC RT viewer my SVG symbols, which i am using from siemens library, disappear and only the logo of SVG symbols is displayed and background color of the screen also turns to black. Please give me the solution as I am beginner in this field. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/06/2024 07:04:24New subject after splitting |
|
8/8/2024 8:46 AM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13803 Rating: (1741)
|
Hello Harry_007 there are a lot of fixes and stabilisations regarding svg in the readmes of V18 Updates. But if you install an update for TIA Portal you also have to install the same update for WinCC Runtime Prof: LINK After installing you will have to run the Webconfigurator again on RT System and do a complete full download again to the system. Also you would be able to download a new version of Webclient/WinCCviewerRt Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on