9/10/2024 8:01 PM | |
Joined: 9/10/2024 Last visit: 9/14/2024 Posts: 2 Rating: (0) |
Good evening I have been working more than a year with logo type 6ED1052-1MD08-0BA1 without problems Now i bought 2 new units type ; 6ED1052-1MD08-0BA2 I'm using LOGO!soft comfort v8.3.0 The firmware of both logo's are 1.84.02 PC is connected with the logo with network cable cat6 (standard cable) IP PC ;192.168.0.13 IP BM ;192.168.0.3 IP TDE;192.168.0.2 subnet all devices ;255.255.255.0 gateway all devices;192.168.0.1 I can see the TDE and BM in software,,connection test on TDE is fine but not on BM Same problem with both new devices, when i connect the old logo (with the same IP settings) he's working fine... I removed the SD card from the old logo and installed it in the new logo's; there are working fine with the program but i can't connect them with my computer Any idea??? Thanks for your support!! ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 09/11/2024 09:46:23New subject after splitting |
|
9/10/2024 8:13 PM | |
Joined: 12/18/2014 Last visit: 11/13/2024 Posts: 34207 Rating: (4261)
|
The upgrade to LSC V8.4 can you download from here: Download and installation instructions for LOGO! Soft Comfort Upgrade V8.4 |
Follow us on