9/27/2024 10:43 AM | |
Joined: 1/20/2022 Last visit: 9/27/2024 Posts: 3 Rating: (0) |
Here is the whole project. as you can see, I use the 4 AI's, scale and copy them to VW's Then I compare these actual temperature VW's with the settings that are made in the LWE project. It al works fine as long as the LOGO is not powered down Hope you can help me with that. Attachmentthermostaat met LWE.zip (88 Downloads) |
9/27/2024 11:57 AM | |
Joined: 1/20/2022 Last visit: 9/27/2024 Posts: 3 Rating: (0) |
Thank you! This is exactly what I needed. Have a nice weekend |
This contribution was helpful to1 thankful Users |
Follow us on